Default Header
(header konnte nicht geladen werden)
(0)| 8/25/2009 9:37 AM | |
|
Posts: 34 Rating:
|
d00, 1) AboutRET_VAL value, If an error occurs when the function is being executed, the "return value" RET_VALcontains an error code. You can find more info here: http://support.automation.siemens.com/WW/view/es/1214574/0/en 2) The built-in solution doesn't exist but you have two solutions at least: a) Make your own "loop function" with the Step7 LOOP instruction b)If youuse a S7-400 you coulduse the fuction SFC26 in order to update the partial process image (updatea PAE partial area)and after that a regular SFC20 call movingthe updatedPAE area Regards |
Follow us on