Default Header
(header konnte nicht geladen werden)
(1)| 10/13/2009 8:31 AM | |
|
Posts: 159 Rating:
|
Thanx again Phantom75. You continue to amaze me with your endles knowledge |
| 10/13/2009 10:27 PM | |
|
Posts: 2661 Rating:
|
Hi Testermax,You do not have to manually move the SFC to OB100 (or any other OB). Set the properties of the initialize SFC as shown in the attached screenshot and give it a try. Please delete your earlier SFC and recreate it. Also, if you want to trigger this SFC under other conditions you need to connect the conditions using external view. And in certain situations the "Retain SFC state" isuseful. BTW, thanks for the ratingand praise before, you are too kind... Regards AttachmentSFC_Init.pdf (495 Downloads) |
Follow us on