Default Header
(header konnte nicht geladen werden)
(0)| 10/13/2010 4:24 AM | |
|
Posts: 71 Rating:
|
Hi, I'm quite new to this. I tried to use SFC21 to clear all the values in the data block, When i tried to Clear DB from 0.0 to 2954.0, it's working fine But however, when i tried to clear starting from 3958.0, It turns out to have an error with the ret_val =-31965 or w#16#8323 From the help menu stated that: Range length error when writing a parameter. This error code indicates that the parameter x is located either entirely or partly outside the range of an address or that the length of a bit range is not a multiple of 8 with an ANY parameter. however, i don't really understand this. Could anyone help me on this? I attached an pdf file which consists of two pictures one is the blocks without error one is the blocks with error. Much appreciate if anyone could lend me a hand. Thank you! cheers, createstars AttachmentERROR.pdf (272 Downloads) |
| 10/13/2010 10:39 AM | |
|
Posts: 1121 Rating:
|
Hi Well are u using the sfc21 "FILL", function. If yes then can you post your program here, so that i can test the same. Have fun.. |
| 10/13/2010 11:35 AM | |
|
Posts: 2348 Rating:
|
What length DB14 has? Also please check that online version of DB14 matches offline. |
Follow us on