Default Header
(header konnte nicht geladen werden)
(0)| 11/26/2010 8:06 PM | |
|
Joined: 9/27/2006 Last visit: 12/29/2025 Posts: 12477 Rating:
|
Hello toufik; Dowloading and uploading from a Siemens PLC is very weel explained in the mmanual "Programming with step 7, v.5.4"; it isavailable on the computer whereyou installed Step 7 (under Simatic, Documentation); you can also dowload it from this link: Programming with STEP 7 V5.4 The "normal" programming port of the PLC is the MPI port (multi-purpose interface), which communictaes over RS-485. You will need some kind of programming cable/lead to communicate from your laptop to the PLC. such as the USB-PC adapter (part number 6ES7972-0CB20-0XA0 ), or a MPI/Profibus communication processor. Note that if you do not have a backup of the program on your PC, you will not retrieve the symbol table or the comments of the program, which tends to make your understanding of the controls quite difficult. Hope this helps, Daniel Chartier |
Follow us on