Default Header
(header konnte nicht geladen werden)
(0)| 5/11/2011 11:06 AM | |
|
Posts: 80 Rating:
|
Hi! Ok,I send you screenshots. And I must admit, that you solved my problem, butI do not understad this: 1, I download your sample program, make the PLC type change. 2, When I right click on the PLC in TIA portal, and choose "Download to device - > ALL" it isdownloaded but does not work.And itcan be monitored, the values of the variables can be changed (that is in myattached file). BUT 1, I download your sample program, make the PLC type change. 2, I rebuild all blocks 3, I right click on the PLC in TIA portal, and choose "Download to device - > ALL" it isdownloaded and works. I have never experienced suchstrange thingin S7-300 and Step7. Is there something like "autobuild" before downloading in it? And if it is, then why does TIA not have it? (I often feel in TIA that some developers have developed very good and usefull thing in Step7, and the new TIA developers does not care, do not use the ideas, starts everythingagain (and forget a lot to develope thanks for the help. Coyote AttachmentDok1.pdf (1053 Downloads) |
Follow us on