Default Header
(header konnte nicht geladen werden)
(0)| 8/1/2011 6:11 PM | |
|
Joined: 9/27/2006 Last visit: 12/31/2025 Posts: 12479 Rating:
|
Hello hazem; If you review the various opinions expressed in the following thread, you will see that you will recieve little help on the forum concerning this issue: /tf/WW/en/Posts/28316 One of the reasons for it is that the 'Ramp' function block that you are trying to open (since this is the one you are pointing at) is one of many pre-programmed blocks from Siemens; as such, they are distributed with the Know_How_Protect lock so that anyone using them will have exactly the same function. All such blocks work the same way, because they are protected. If anyone could open them, there is a risk of modifyng them(willingly or not) and then programs using this block will work differently (if at all) than 'standard' blocks of the same name. You might find ways to open these blocks on the web, if you search adequately, but I strongly suggest you be very prudent in the way you handle an unlocked functionblock. Hope this helps, Daniel Chartier |
This contribution was helpful to
|
|
Follow us on