(0)| 2/14/2007 2:50 PM | |
|
Joined: 8/31/2005 Last visit: 1/7/2026 Posts: 217 Rating:
|
There are some examples, that use OPC to transfer data to a SQL server: PC-Based Automation: Connection of Databases via open Interfaces Using OPC-XML, Programmed in C# .net Mass Data Acquisition with an OPC Client in C# based on .NET |
|
Greetings, Chris |
|
| 2/15/2007 11:57 AM | |
|
Posts: 5822 Rating:
|
Hello, I am sorry, for the configuration of the Connection with STEP 7 I have no Sample handy, but it is not that difficult. You have to add the OPC Server to your PC Station in HW Config. In NetPro you have to create a S7-Connection form the OPC Server to the WIN LC and that’s it. AttachmentPc_station1.zip (880 Downloads) |
Last edited by: J_Bell at: 2/15/2007 12:19 PMThe Attachment contains a little Project with WinLC; OPC Server and a S7 Connection in between, maybe this will help. |
|
| 2/16/2007 11:10 AM | |
|
Posts: 3 Rating:
|
Hi. Bill I have configured the OPC server in my S7 project... kindly have a look at the attachement and guide me futher... with best regards Muralidhar.BR AttachmentConfiguration.pdf (1027 Downloads) |
Follow us on