3/12/2012 12:46 PM | |
Joined: 7/7/2010 Last visit: 9/12/2025 Posts: 16094 Rating:
|
TIA Portal installation and many other tasks like migration do not allow \\tsclient\c or UNC paths for file locations. Map a drive in XP Mode to \\tsclient\c and it should work as expected. If you create a persistent mapping to that drive, it should always appear (after a brief pause after vm startup) and be available. Starter is the same way, so the presumption on my part is the same installation restrictions apply throughout much of the automation product line, and should be no surprise for 'in-application' file i/o either. Yes, it would be nice if it allowed UNC paths! |
science guy |
|
Follow us on