Default Header
(header konnte nicht geladen werden)
(0)| 5/30/2012 6:19 PM | |
|
Posts: 10 Rating:
|
Hello First of all, thank you so much for the example Pegaia. It is very helpfull. I'm trying to understand wich is the correct procedure/line of commands but i wasn't successful yet.. My goal is to storage 4 values every day in the data log. At the end of every month, it must create a new data log with ID of the correspondent month. The same goes for 12 months = 1 year. I was thinking i could use the system_time and read the days, months and years from it and use it on the ID's (not sure if that's the right way to do it). After 2 years, the data log will be replaced for new data (don't have any external memory, only the PLc's, so i wonder if the PLC memory (i'm using the 1212C CPU) is enough to accomplish what i need?). Can anyone please explain me how can i accomplish this? And wich is the correct line of commands i must execute to do so? Thank you so much. EDIT: I already found a valid example on the System Manual - Chapter 8.7.5. My question is: If i only need to create a data log to download via Web Server, i only need to use the CREATE, WRITE and NEW FILE functions right? Thanks |
Last edited by: O_Moderator at: 6/11/2012 9:32 AMnew subject after splitting from /tf/WW/en/Posts/57715#top Last edited by: Tiago Soares at: 5/30/2012 6:27 PM |
|
Follow us on