Default Header
(header konnte nicht geladen werden)
6/25/2012 11:41 PM | |
Joined: 10/7/2005 Last visit: 9/14/2025 Posts: 3049 Rating:
|
Hello DLittlejohn412 ENO is simply a reflectionof the status of the BR bit (Binary Result bit), so your code should look like this (Note too that you can not use "L" and "T" instructions on Booleans): A BR // Check BR bit (=ENO of preceeding FC call) ="TE_01".VALID // /assignBR bit to Bool variable I hope this helps |
Cheers |
|
This contribution was helpful to
2 thankful Users |
Follow us on