Default Header
(header konnte nicht geladen werden)
7/14/2009 5:23 PM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Hello, In my opinion theReport System Error is the best choice. As actually you do not make any thing excepts few setting through a wizard of RSE. The details are here in this FAQ and you also told that you are aware of it. How can you report S7 system errors in WinCC? So If the issue that you have to buy a new licence to integrate your WinCC in Step 7. I think you are the winner as you will save in engineering time. As you won't have to implement each error and create message in WinCC specially if you are talking about large project. It will consume a lot of time. But with RSE, just few minutes will do the job. |
Ayman Elotaify |
|
7/15/2009 6:42 PM | |
Joined: 3/24/2009 Last visit: 8/7/2023 Posts: 406 Rating:
|
Hi... I am also trying for the same.... Now i am trying with SFC51 using this we will get all the diagnostic... Search in the forum "SFC51" u will find lot of solution... I will also attach you the some example using SFC51 for your reference..... Hope it help u... AttachmentEXAMPLE.zip (226 Downloads) |
All is well :-) |
|
Follow us on