8/16/2012 12:20 AM | |
Posts: 14 Rating:
|
Hi, I have a problem with the use of analog inputs of S7 300, I must declare these inputs as for example EW256 or PEW 752 ?? thank you very much |
8/16/2012 12:02 PM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
And as an addition, when using EW, the address should be inside the process image of the CPU. Please see this FAQ:Where and when do you need peripheral addressing?
|
Ayman Elotaify |
|
This contribution was helpful to
1 thankful Users |
8/19/2012 11:41 PM | |
Posts: 14 Rating:
|
thank you very much, when I changed the type WORD by INT the problem is resolved. |
This contribution was helpful to
2 thankful Users |
Follow us on