Default Header
(header konnte nicht geladen werden)
8/22/2012 2:10 PM | |
Posts: 288 Rating:
|
hello. there is code like below in ob1 of most plc programs. A M 0.0 R M 0.0 AN M 0.1 S M 0.1 What are these bits(m0.1 and m0.0) used for? best regrads.
|
8/22/2012 2:39 PM | |
Posts: 288 Rating:
|
hello. what is usage and advantage of using these bits? best regards.
|
8/22/2012 2:47 PM | |
Posts: 197 Rating:
|
@ saeedplc : "...what is usage and advantage of using these bits?" check the occurences of M0.1 and M0.0 in your program ........ particularly where they are used and in which functions of the machines or process. Righ click (on these bits individually)--> Go To --> Locations = this will take you to all networks where these bits are used. you need to understand those networks wherever these bits are used and what function that network does on your machine / process. you don't have symbollic information? Regards |
8/22/2012 3:01 PM | |
Posts: 288 Rating:
|
thanks for your reply. "always one bit" has been used for call of most fc and fb . A m0.1 cc fc1 and also on "en" of most fc and fb best regards.
|
Follow us on