Default Header
(header konnte nicht geladen werden)
(0)| 5/17/2007 1:08 PM | |
|
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hi, I don't know which Ethernet communication can be used for Omron but the next will work always when you can built up a connection from the Omron with TCP/IP. With OPEN TCP/IP you may do that, look on the example thats on the page OPEN TCP/IP Examplelook also in the handbook System Software for S7-300/400 System and Standard Functionsfor more information about the useable functionblocks. |
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on