Default Header
(header konnte nicht geladen werden)
3/26/2014 9:27 AM | |
Posts: 1299 Rating:
|
Hello, for first issue you can definea plc tag as acknowledge tag. use the same tag on both hmis. for second and third issue maybe it's an option for you to update to wincc v13? working with step7 v5.5 and v13 is a lot easier! see the first document in this article: http://support.automation.siemens.com/WW/view/en/73502293 Alternatively you can use the system function "Change connection" to switch the communication partner. K!ke |
3/26/2014 10:01 AM | |
Posts: 47 Rating:
|
Thank You K!ke for your response The issue is how i'm gonna decide wich CPU is working and which is out of order. I need Info about active cpu!!!! Regards Rai |
3/27/2014 3:59 PM | |
Posts: 1299 Rating:
|
Hello, see this topic: /tf/WW/en/Posts/100483 K!ke |
4/3/2014 10:44 AM | |
Posts: 515 Rating:
|
hi, why dont you try the methods in below thread? |
Last edited by: S7 AUTOMAN at: 4/3/2014 10:53 AMLast edited by: S7 AUTOMAN at: 4/3/2014 10:47 AM |
|
4/3/2014 12:26 PM | |
Posts: 515 Rating:
|
hi, For the H status why dont you use the FB523 Status H-System block? See the attachement in the below link? is that waht you require? |
Follow us on