Default Header
(header konnte nicht geladen werden)
(1)| 7/28/2013 12:53 AM | |
|
Joined: 9/23/2005 Last visit: 12/28/2025 Posts: 4434 Rating:
|
Hi, one of the inovations of the SP1 for STEP7 V12 (Released for Delivery at http://support.automation.siemens.com/WW/view/de/76276623) is the User data types on I/O area. Here there is a very simple sample project to ilustrate how it works. Two data types was created to group PROFIdrive Standard Telegram 1 (one as inputs, other as outputs). It is possible to see the feature in the simble table, OB1 and watch table. Note: this sample program has the target to exemplify User data types. It is not intended to be a sample program about drive control via PLC.
AttachmentStruct IO.zip (467 Downloads) |
|
Denilson Pegaia |
|
This contribution was helpful to
|
|
| 5/12/2014 8:45 AM | |
|
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
New question splitted to Why udt element have linear scaling property? Best regards O_Moderator |
Follow us on