Default Header
(header konnte nicht geladen werden)
7/7/2014 3:59 PM | |
Posts: 1299 Rating:
|
Hello, please give us some more information about the configuration and the behaviour when error occured K!ke |
7/8/2014 9:52 AM | |
Posts: 2 Rating:
|
Have not accessed the PLC yet. But, as of now, the machine is not functioning at all because of the SF fault on the PlC. The PLc is 315-2DP. |
7/8/2014 12:57 PM | |
Posts: 1299 Rating:
|
Hello, there are many possible reasons for the sf led. I don't think anyone here is able to help you without more information. read out the diagnostics buffer of the s7... if it's urgent ask siemens supportto help you. but they'll also need some more information. K!ke |
Follow us on