(0)| 8/10/2014 11:44 PM | |
|
Posts: 11 Rating:
|
Hi I have s7-1200 1212C AC/DC/Relay It is a good isea to check the input voltage: Logic 1 signal (min.) 15 VDC at 2.5 mA Logic 0 signal (max.) 5 VDC at 1 mA ProbablyI willneed to install a load (resistor) as indicated before.Theproduct technical doc pg A-59 is mentioning load (for relay). Also on A-62 is written "Do not connect the power supply to the sensor with no load connected..." So the resisitor is needed probably, I´ll check the voltage first. Link to technical document: http://ee.farnell.com/omron-industrial-automation/e3z-d81-2m/sensor-100mm-diffuse-dc-pnp-cable/dp/1909108?Ntt=omron+E3Z-D81 Or do I use also M1 digital input on the controller. I see from the sytem manual S7-1200. And thanks, of course... |
Last edited by: Madis_M at: 8/11/2014 12:12 AMLast edited by: Madis_M at: 8/11/2014 12:10 AM |
|
Follow us on