Default Header
(header konnte nicht geladen werden)
4/30/2012 4:16 PM | |
Joined: 7/7/2010 Last visit: 9/12/2025 Posts: 16094 Rating:
|
1. Where do you find the data defining the infromation? I googled "singeturn version 2.2 gsd" and found a link toa pdf that may be helpful: https://www.automation.siemens.com/doconweb/pdf/SINUMERIK_SINAMICS_04_2010_E/BHA.pdf?HTTPS=REDIR&p=1section 3.2
The manuals says there is a "user friendly configuration tool"!! I suggest you check with your local Siemens applications engineering folks to get your hands on that. 3. If you want to read/write acyclic parameters after the device is configured and working, yes, you will need to write the plc logic to handle read/write from/to the device. Maybe you are really asking about the user friendly configuration tool mentioned in the manual? |
science guy |
|
4/30/2012 6:29 PM | |
Posts: 150 Rating:
|
As soon as I get my hardware delivered I will setup an example and post it in the forum. Thanx |
Follow us on