(0)| 7/19/2015 4:39 AM | |
|
Posts: 5 Rating:
|
Hello Denilson thanks for the link . I have tried today to Update my package for TIA V13 and it shows V13 SP1 Update 3 .After which I have installed the PLCMSIM V13 . online access tabs shows PLCSIM and PLCSIM S7-1200/1500 . I have complied the program and when I try and check for starting the simulator the start is disabled . The project consist of S1200 two modules and two KTP 600 HMI . The start simulator is enabled for HMI but not for the CPU 1214C . Fail to understand why , any help ---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/20/2015 11:48:26 AMNew subject after splitting |
|
Follow us on