(0)| 4/29/2008 6:41 AM | |
|
Posts: 487 Rating:
|
Hi If the comms port is not working then working via the ethernet card is not possible . In Step5 you can define a Path Have a look under Editor .. Bus Path ..Edit .. then select a file name for and then a name for the Path ( ie Test01AP.INI and PLC01 for Path) Then in EDIT build up you path start with PG/AS511 then CP-H1.. CP-H1 ..ENDP , you have to fill in you mac adress or IP adress ( if working with a TCP/IP card) If you have to fill in the IP adress ( in Hex) then start from the first digit and leave the last four digits empty btw ; what 928 CPU do you have .If you have a 928B then you could use the second submodule with a PG interface card. Another point : You said that the old TTY interface worked with a external power supply .Speaking under correction Looking at the pin lay-out page 11-15 the interface has a 24v powersupply ,you could check if the interface is giving 24v if not then use an external supply .Have a look at the following document ,its from Phoenix ( don't shoot me ) and explains the active passive stuff Hope it helps Eric |
Last edited by: aikona at: 4/29/2008 7:03 AM |
|
Follow us on