4/4/2017 8:30 AM | |
Posts: 16 Rating:
|
You can use ethernet switch or router to connect your PC and IOT2020 to network and inernet |
This contribution was helpful to
1 thankful Users |
4/4/2017 10:25 AM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
You also can use a WIFI-USB Dongle if you have a WIFI router. For example this one: http://de.rs-online.com/web/p/wireless-adapter/8920012/ It works by plug&play and you can configure the WIFI via "iot2000setup" Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to
1 thankful Users |
4/27/2017 7:21 AM | |
Joined: 2/20/2014 Last visit: 9/3/2025 Posts: 405 Rating:
|
Hi, thanks for your reply. Can i know how i can configure the WIFI via IOT2000setup? What are the settings that need to be done? Is there any document for this? Besides, i have setup a connection like below mentioned but unable to ping www.google.com D-link wifi router with DHCP internet connection where i have connected a LAN cable (RJ45) from the router to a Ethernet to USB converter & connected the USB to the IOT2020 USB port & another ethernet cable from laptop to IOT2020 ethernet port. Please advise further. Thank you in advance.
|
5/2/2017 3:58 PM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, check out this FAQ: https://support.industry.siemens.com/tf/ww/en/posts/how-to-add-usb-wi-fi-connection/159113/?page=0&pageSize=10. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on