(2)| 3/10/2006 3:11 PM | |
|
Joined: 8/31/2005 Last visit: 1/7/2026 Posts: 217 Rating:
|
Hi nkraven! Since the Firmware V2.4 contains only error corrections (see here: http://support.automation.siemens.com/WW/view/en/17504794) and no additional functionality, you can use the V2.3 from the hardware catalog to configure you CP 443-1. If you have no V2.3 in your hardware catalog, you should install the hardware updates from the internet (in the HW config editor via "Options -> Install HW Updates ...") |
|
Greetings, Chris |
|
| 3/13/2006 10:50 AM | |
|
Posts: 5822 Rating:
|
Hi nkraven, |
| 3/14/2006 8:31 AM | |
|
Posts: 15 Rating:
|
i updated the firmware version with the file that you recommended and it works now. Thank you for you support. Best Regards nkraven |
| 5/11/2018 6:42 AM | |
|
Posts: 8171 Rating:
|
New question published by Siemens-man is split to a separate thread with the subject How can add the CP443-1 (6GK7 443-1EX30-0XE0) to the SIMATIC MANAGER?. Best regards |
Follow us on