(0)| 5/13/2018 9:32 PM | |
|
Joined: 9/27/2006 Last visit: 1/2/2026 Posts: 12479 Rating:
|
Hello; What version of Windoews does the new PG run with? The drivers for the CP 5412 A2 can run on Windows 3.0, Win 95, Win NT4.0. It uses an ISA connector, ont available on newer Pcs. The Simatic Net software for FMS also were limited to Win98 and NT 4.0. See the following document and the screenshot below, about requirements for the CP 5412 A2.: https://www.itk.ntnu.no/fag/TTK4175/Lab/Profibus/Profiman1.pdf On the other hand, here are the system requirements for Step 7 v5.5: System requirements Supported operating systems:
https://support.industry.siemens.com/cs/ww/en/view/44370501 How is your PG setup for FMS communication? Does it have the standard CP 5611 chip for Profibus, or is there an additional CP for FMS connections (it requires an additional Simatic Net driver in that case). Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 5/13/2018 9:37:19 PMLast edited by: dchartier at: 5/14/2018 2:53:17 AM |
|
Follow us on