(1)| 6/7/2018 3:57 PM | |
|
Joined: 10/1/2013 Last visit: 12/23/2025 Posts: 605 Rating:
|
Hello Alexey, I'm afraid there is no specific application example for your purpose. What can you do? Get the block "Ident_Profile" (FB1900) from this example (download the STEP 7 V5.5 project): To use it just copy the block to your project and call it. Also copy the data types "IID_HW_CONNECT" (UDT1900) and "IID_CMD_STRUCT" (UDT1901) because you'll need them. Ignore the others blocks. They're related to RFID readers. To understand how to control the inputs and outputs of this block you can read the manual: The standard block is described in chapter 3.5. Also note chapter 3.5.4.3. This chapter explains the commands for MV4xx code readers. I hope this helps :) |
This contribution was helpful to
|
|
Follow us on