(0)| 7/19/2018 12:39 PM | |
|
Joined: 6/30/2017 Last visit: 8/21/2024 Posts: 1 Rating:
|
I have problem with HW config. in Step7 5.6 . I have IM155-6 PN ST v3.3 product code of IM: 6ES7155 6AU00-0BN0 . I donwloaded PROFINET GSD files: I/O - ET 200SP from siemens site. Now i have GSDML-V2.33-Siemens-ET200SP-20171130.xml . And in my project there are Digital F-input modules , but in the library FDI is missing ! Product code of FDI: 6ES7136-6BA00-0CA0 So I am not sure if i can use that IM for F-modules, but in description is that F modules are included. But i can´t complit HW confing. because F-module is missing in library. There are 2 of 6ES7155 6AU00-0BN0 in library one includ the F-module but missing DI module 6ES7131 6BF01-0BA0 . Both of these version are not complited. Do you have any idea what can i do? Attachmentim155-6 PN ST v 3.3.zip (408 Downloads) |
| 7/20/2018 9:16 AM | |
|
Joined: 2/11/2015 Last visit: 12/18/2025 Posts: 515 Rating:
|
Hi, Maybe you need the package: |
Last edited by: Jen_Moderator at: 7/20/2018 11:31:33 AMOptimized link. |
|
Follow us on