(0)| 8/27/2018 11:06 PM | |
|
Posts: 1 Rating:
|
totally confusing CPU 315 2 DP total program cycle ~28ms OB 35 set to 5ms first instruction in OB 35 is call periphery PEB and load to EB there after several ADD and SUB networks are programmed for fast impulse counting all working fine only the first network after the periphery refresh is causing intermitted problems by not counting now I programmed an additional network between the periphery refresh and the first ADD / SUB network with the ROL_1 and it works all counters behaving well am I dreaming ??? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/28/2018 6:28:46 AMNew subject after splitting |
|
Follow us on