Default Header
(header konnte nicht geladen werden)
9/11/2008 10:25 AM | |
Posts: 3 Rating:
|
Hi all, I am able to generate PULSEOutput with my S7 - CPU 313 C - 2 DP. At present i have configuredIn Hardware Configuration. Its ok but when i gone thru the manual from the given site http://support.automation.siemens.com/WW/view/en/12429336i came to know from its 256 th page as shown in th picture the parameters can be changed from SFB also. But In SFB 49 i am unable to find the option for changing Period, On Delay, Minimum Pulse Width. Is there is any other SFB shall be used? Even if we use SFB then what is the parameter to be set in Hardware Config? Please Help.. Thanks... Jack |
Follow us on