Default Header
(header konnte nicht geladen werden)
9/19/2008 1:46 PM | |
Joined: 7/15/2008 Last visit: 3/13/2025 Posts: 382 Rating:
|
Hello , Yes you can , Please type " Uploading " in Step 7 Help Index and follow the Procedure. |
9/19/2008 2:20 PM | |
Posts: 487 Rating:
|
Lukaz, Uploading the project will not bring the HW version to STEP7. You can have the uploaded project as a backup. To update your HW catalog in Step7 you need to install the updates which is free and available over internet. Check these two links below. http://support.automation.siemens.com/WW/view/en/17581199 http://support.automation.siemens.com/WW/view/en/24787694 |
Follow us on