Default Header
(header konnte nicht geladen werden)
(0)| 6/8/2019 6:01 PM | |
|
Posts: 35 Rating:
|
there are DBs in one project that when i open it and make it online there is two column with @actual value bule colored and other actual value and white? why is like that? and when i change a input that goes through this db with modbus protocol to another system only @actual value blue colored changes and in other system nothing receives. why this happens? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/11/2019 09:00:02New subject after splitting |
|
| 6/13/2019 7:13 AM | |
|
Posts: 623 Rating:
|
Hi saba_149, Can u share the snaps of DB ?? U can use context sensitive help. 'Select & Press F1' |
Follow us on