(0)| 1/14/2020 5:38 PM | |
|
Posts: 1 Rating:
|
Hi Christoph, Would a firmware mismatch cause an error in the Diagnostic Buffer to read the following? "PG Start command was denied due to inconsistent or missing database, external error, incoming event." I have a similar situation of the device firmware as v3.1.1 with GSD v3.0 but cannot get the CP343-1 to Run, stuck in Stop. I will also note that I'm using Step7 (Classic) v5.5+SP4+HF11. ------------------------------------------------------------------------------------------ |
Last edited by: hbhosch2 at: 01/14/2020 17:41:58Last edited by: The Helping Hand at: 01/15/2020 14:24:05New subject after splitting |
|
Follow us on