(0)| 6/22/2020 7:47 AM | |
|
Joined: 9/30/2016 Last visit: 1/12/2026 Posts: 953 Rating:
|
Hello dchartier, Thank you for answering. Please also see the screenshots. I am pretty sure the author is a user (not a Simatic predefined block) from the company who originally programmed the machine control for us. As you can see in the screenshot a LOT of blocks have no author listed. When I position the cursor over the "in_value" pin I get the answer OUT: BOOL which also makes sense since this output is connected to DBxx.DBx.x values in the datablock. And therefore I think I SHOULD be able to put an AND-block on the pin?
AttachmentFC357.zip (225 Downloads) |
Follow us on