(0)| 8/14/2020 4:58 AM | |
|
Posts: 112 Rating:
|
HI All, I used siemens support example to transfer data from my PLC s71500 using as a OPC Server to my PC directly in to the excel. I have downloaded all the manual and the excel from siemens, Entry type:Application exampleEntry ID:109748892,Entry date:06/10/2020 https://support.industry.siemens.com/cs/us/en/view/109748892 All communication are excellent for except when I use UDT datatype in the ReadStructUdt, The UDT data is only updated when I click on the button but cannot update cyclically. May I know how to accomplish this. Also In the subscribe tab cyclic acquisition of data occurs with single tags. The problem is only with the UDT tags. Attached the EXCEL sheet. Thankyou Attachment109748892_OPC_UA_ClientLibrary_Sample_V2_1.zip (306 Downloads) |
Last edited by: Jen_Moderator at: 08/17/2020 12:04:39Optimized link. |
|
Follow us on