(1)| 10/22/2020 2:52 PM | |
|
Joined: 1/28/2009 Last visit: 1/5/2026 Posts: 6892 Rating:
|
Dear user,
You can keep Critical parameters that are related to safety of the machine in a DB and it is wise to update the initial values after any necessary limit change. Limits should be checked if they are plausible, deviations should not be tolerated. It is also possible to make the initial values in effect for parameters that are not overwritten in the program. STEP 7 classic doesn't have the option to capture the critical process values but the available options is using logging packages, uploading the updated project. Also check the following link in the forum: https://support.industry.siemens.com/tf//ww/en/posts/datablock-backup/55171?page=0&pageSize=10 I hope it helps, hdhosseini |
Last edited by: hdhosseini at: 10/22/2020 14:52:47 |
|
| 10/23/2020 12:36 PM | |
|
Joined: 9/21/2012 Last visit: 1/15/2026 Posts: 4848 Rating:
|
Did you look into the proposal i gave you in your other post? |
Follow us on