Default Header
(header konnte nicht geladen werden)
(0)| 1/20/2009 8:46 AM | |
|
Joined: 9/27/2006 Last visit: 1/12/2026 Posts: 12480 Rating:
|
Hello HiLimit; Sorry, the only examples I know or the use of FC105 "SCALE" is found in the online help of Step 7. Look for it. There is also the following FAQ that provides additional explanations on the different input and output parameters of the function: http://support.automation.siemens.com/WW/view/en/1765297 Hope this helps, Daniel Chartier |
Follow us on