9/5/2006 12:05 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
I've seen this a few times before. Below are somethings that have fixed it : - Ensure you can ping the server on both IP address and computer name - Ensure the SIMATIC Shell folder llists the server andproject state correctly on the client - Hardcode the network speed on the network cards on both client and server - Delete server data package, check file is deleted in Windows Explorer and recreate package - Ensure the exact same version of WinCC is on client and server - Try creating same username / password on both client and server, add the user to the Windows SIMATIC HMI and Administrator groups and log-on using this user (more information on this at http://support.automation.siemens.com/WW/view/en/22784251) - Check both computers are using the same timezone and clocks are synchronised - Check both computers have same language configured in Control Panel -> Regional Settings ( remember if it's English then it must be English(US) and not English(UK) ) This is not a complete list, just what I can think of right now. Hopefully one of them will work for you. |
This contribution was helpful to
1 thankful Users |
9/5/2006 12:29 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
Also, if you are using DNS please read this thread - WinCC SP4 |
9/5/2006 1:42 PM | |
Posts: 62 Rating:
|
[quote user="salma"]I've seen this a few times before. Below are somethings that have fixed it : 1. Ensure you can ping the server on both IP address and computer name 2. Ensure the SIMATIC Shell folder llists the server andproject state correctly on the client 3. Hardcode the network speed on the network cards on both client and server 4. Delete server data package, check file is deleted in Windows Explorer and recreate package 5. Ensure the exact same version of WinCC is on client and server 6. Try creating same username / password on both client and server, add the user to the Windows SIMATIC HMI and Administrator groups and log-on using this user (more information on this at http://support.automation.siemens.com/WW/view/en/22784251) 7. Check both computers are using the same timezone and clocks are synchronised 8. Check both computers have same language configured in Control Panel -> Regional Settings ( remember if it's English then it must be English(US) and not English(UK) ) This is not a complete list, just what I can think of right now. Hopefully one of them will work for you. 1. I can ping both computers by IP and computer name 2. Client see HMIPAS1 and Omega_Server project (Status: Run Time when project is activated) 3. "Hardcode the network speed on the network cards on both client and server" Sorry but I dont understand what does this mean [:(] Set speed, in my case, to 100 Mbps? 4. Done. 5. All good. 6. All good. 7. All good. 8. Checked. ----------- Sorry for changing your original quote, I made changes for easy understanding. All things are OK but I get same error [:cry:] |
This contribution was helpful to
1 thankful Users |
9/5/2006 3:40 PM | |
Posts: 62 Rating:
|
Firewall and antivirus are off. OS is Windows XP Pro SP2. Is there any other step-by-step manual for setting-up client-server arhitecture? |
9/7/2006 2:18 PM | |
Posts: 62 Rating:
|
Sorry for my ignorance, I don't know what can I see there. I'm sending You screenshot of that part. |
9/7/2006 2:48 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
oh dear, better you got [:mad:] |
9/7/2006 2:53 PM | |
Posts: 62 Rating:
|
Thank You, I will try [:)] |
Follow us on