8/1/2010 6:43 PM | |
Posts: 10 Rating:
|
Thanks BilaID and Fade UP. If "Name connection" is not type protocol, why it is into "SIMATIC S7 PROTOCOL SUITE"? Can you explain more for me? |
8/2/2010 3:43 AM | |
Posts: 10 Rating:
|
I'm understand Fade UP. :) Thanks. |
9/14/2010 2:02 PM | |
Posts: 241 Rating:
|
There is no possibility to connect Tags under Named connection with PLCSIM.One way to do is to move the tags from Named connection to MPI. This can by done by: 1. Open WinCC Project 2.Open SQL Server Management Studio 2005, my case 3.Connect. 4.Then Open Database as attached-"Table1" 5.Then Exchange the channelnumber value as arrow marked in in the 2nd pic.CHUNITNUMBER 6. Now check Tag are exchanged between MPI & Named connection. There may be difficulty doing with Structured tag, but may be some way should be there. This is just a way, not professional way to do.
AttachmentTable.zip (1410 Downloads) |
This contribution was helpful to
8 thankful Users |
7/1/2014 11:21 AM | |
Joined: 9/1/2005 Last visit: 8/22/2025 Posts: 4114 Rating:
|
|
My Forum is the place to personalize your profile, |
|
7/5/2014 10:31 AM | |
Posts: 49 Rating:
|
Hi, |
11/20/2015 3:29 AM | |
Joined: 3/8/2013 Last visit: 4/7/2022 Posts: 11 Rating:
|
Hello! Sorry! Where is second picture? |
Follow us on