10/10/2007 11:48 AM | |
Posts: 21 Rating:
|
Dear All, I have CPU226 and SIEMENS FIELD PG. In the early days, I used field pg to download, modify and upload through CP5611 PCI Slot, which is inbuilt in FIELD PG. But one day, I tried to communicate CPU226 with PC/PPI-USB type cable, it is not communicating. Of course, I changed PG/PC Parameters to PC/PPI Cable and LOCAL CONNECTION - USB. No communication. Even I tried with PC/PPI-RS232 Type cable. Still no communication. If I tried to communicate, it shows an error, which I have attached in this thread. Can anybody please give me the solution? Can you please where the problem is? Because I need to give PC/PPI cable only to the customer to communicate with CPU226. Please it is very urgent. Thanx in Advance. Regards, M. Ashokkumar Dubai AttachmentMicrosoft Word - PPI.pdf (616 Downloads) |
10/15/2007 4:35 PM | |
Posts: 4 Rating:
|
Is this the only plc giving you the problem or have you tried the USB cable on another plc? If you have a problem on other plc's, that rules out a problem with plc's. If it is on one and you have the program saved, try "WIPEOUT.EXE" on the plc, reconnect and download the program back. I have attached WIPEOUT. It will flush the 226 with defaults. Good luck and let me know if it works. Attachmentwipeout.zip (527 Downloads) |
10/16/2007 10:21 AM | |
Posts: 21 Rating:
|
Thank you for your help. |
10/16/2007 1:56 PM | |
Joined: 9/29/2005 Last visit: 7/16/2025 Posts: 313 Rating:
|
Hi, is this issue now completed successfully? |