6/5/2011 6:46 AM | |
Joined: 10/7/2005 Last visit: 8/28/2025 Posts: 3049 Rating:
|
Hello Lucky123 silly question: Have you tried to update yoru HW catalogue? How do you update the STEP 7 hardware catalog in STEP 7 V5.2 onwards? STEP 7 Hardware Support Packages (HSPs - as at 04/2011) for installing hardware updates in the Hardware Configuration |
Cheers |
|
6/6/2011 5:38 AM | |
Joined: 12/20/2008 Last visit: 7/15/2025 Posts: 556 Rating:
|
Hi Fritz, As I mentioned the laptop in which I created the project, I myself installed the software and updated the H/W configuration. However, due to some reason that laptop I had to loose. Hence I finally installed the setp 7 into another laptop and opened the application then I got the error1 as in the first post. Subsequently when I updated my hardware configuration, I got the second error in which is also attached in the zip file of the first post. I followed the same step both times. However, I checked the above link sent by you, and followed it through, and still have the same issue. Please advise.
|
6/6/2011 8:23 PM | |
Joined: 12/20/2008 Last visit: 7/15/2025 Posts: 556 Rating:
|
Whole day tried each possibility mentioned in this forum, attached is hw config, problem is still unresolved. I do have another question though. if i have opened the hw config, and did not make any change, and then hit the save button, instead of save and coimpile, will there be any impact, later i hit save and compile. but i heard its a bug in siemens , one should never hit only save button, instead one should always hit only save and compile. please also clarify about it.
Attachmentsimatic 300(1).zip (241 Downloads) |
6/7/2011 8:22 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating:
|
Hi Please find the attached project Have fun... AttachmentTest_1.zip (227 Downloads) |
Jazz |
|
Follow us on