4/1/2020 2:23 PM | |
Joined: 2/16/2017 Last visit: 7/23/2025 Posts: 36 Rating:
|
Hi all. I have the same problem with WinCC Runtime Professional V16. Runtime advance work good no problem but professional dosent work. When ı try start simulation I get "Failed to start Runtime simulation" fault. I tried delete IM folder and rebuild all but problem continue. I didnt solve problem yet. Whats your opinion and suggestion this problem. Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/02/2020 07:18:42New subject after splitting |
|
4/1/2020 5:44 PM | |
Joined: 2/16/2017 Last visit: 7/23/2025 Posts: 36 Rating:
|
Hi AmolG, I tried change the version but its not possible. There is only V16. version. I attached picture. AttachmentWinCC_Prof_Vers.zip (1655 Downloads) |
4/1/2020 6:20 PM | |
Joined: 2/5/2013 Last visit: 8/28/2025 Posts: 326 Rating:
|
Hi frkn001 , Is it possible to you to give information regarding 1.Which windows build installed on your PC. 2.Which TIA Software installed on PC (Snapshot from Installed Software). 3.Attach Snapshot for error (When you starting Run time). 4.Try to create different new WinCC project and start Run time simulation. 5.Is there any previous TIA WinCC Professional software installed on your PC e.g TIA 15.1/15 . If yes may be these files are not properly uninstalled from your PC. Br, AmolG
|
Last edited by: AmolG at: 04/01/2020 18:34:17Please rate it. |
|
4/1/2020 8:15 PM | |
Joined: 2/16/2017 Last visit: 7/23/2025 Posts: 36 Rating:
|
Hi AmolG, Thank you for your reply. I tried the create new WinCC Prof project, but the problem occur again. There is no previous TIA WinCC Professional software installed on my PC. I formatted my PC two days ago and I did clean installaton TIA software. I attached the snapshot,installed software and error messages in the attachment. Thank you again. AttachmentWinCC_Prof_Errors.zip (1521 Downloads) |
4/2/2020 8:11 AM | |
Joined: 2/5/2013 Last visit: 8/28/2025 Posts: 326 Rating:
|
Hi frkn001, Please click on [snip] for sample program.I have tested it on my system and it is working well. Kindly test it on your PC and check whether it is working or not. If yes then there may be problem in your previous project configuration. If no then there will be problem in your software installation. Br, AmolG. AttachmentTIA16_WinCCProf.zip (1598 Downloads) |
Last edited by: Jen_Moderator at: 04/02/2020 12:42:04Removed link and added file as an attachment. Please rate it. |
|
4/2/2020 11:33 AM | |
Joined: 2/16/2017 Last visit: 7/23/2025 Posts: 36 Rating:
|
Hi again AmolG, Thank you for your help. I tried your sample program but unfortunately I got same error. Maybe you're right. Problem is my PC or my windows. Because same software (TIA16 Prof) installed my friend PC and working good. But my PC not working. In addition I have one question. I attached snapshot. Question is, in WinCC advance software RT button active and I use this button. But WinCC prof RT button is inactive and start simulation button active. Whats the difference between them. Thank you. AttachmentSnapshot.zip (1420 Downloads) |
4/2/2020 2:42 PM | |
Joined: 2/5/2013 Last visit: 8/28/2025 Posts: 326 Rating:
|
Hi , This Link may help you !! "To be able to use the configure system to the full and start Runtime, you need the corresponding panel and WinCC Runtime Advanced or WinCC Runtime Professional. Furthermore, in the Engineering system you have a simulation which you can use to test the functions used in the project. The exceptions to this are functions which access the file system of an HMI Panel " WinCC Runtime Advanced and WinCC Runtime Professional are different. Br, AmolG. |
Last edited by: Jen_Moderator at: 04/03/2020 07:15:40Optimized link. Please rate it. |
|
8/17/2021 9:04 AM | |
Joined: 11/14/2012 Last visit: 10/28/2024 Posts: 8 Rating:
|
hi Mohamed AboDaif your solution was very good and useful. Thanks |
Follow us on