9/13/2016 8:54 AM | |
Posts: 11 Rating:
|
Got an old 0BA6 (220v), one Pir sensor (220v) and two light’s ( 220v) Pir notice, people moving, will set a timer for the lights , every time movement is noticed, the timer is set again and again until no movement. than timer count down, and light switch off Before 22.00, two light will be switch After 22.00 only 1 light will be switch ( just a supporting light for walking to the fridge ) Funny thing is, when only 1 light is switch the pir works fine, everytime movement is recorded the timer is set, and the light will be on. But ( before 22.00) when the two lights will be switched, the pir does not work well! The timer is set, the pir does not notice movement until the timer is countdown to zero. so only with one light/load everything works wel, with two lights/load pir does not work wel 1ste light about 60watt, 2de light 100watt ( dimmed ) Hope my problem is a little clear ? English is not my native Anybody a idea about this ? Thanks in advance Alex AttachmentSmall House Tmr.zip (378 Downloads) |
Last edited by: Alex 0ba8 at: 9/13/2016 9:30:23 AM |
|
9/13/2016 9:21 AM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35964 Rating:
|
Please upload your program to the Forum. |
9/13/2016 9:36 AM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35964 Rating:
|
And where is the program? Or have you programmed over display and have no lsc file? |
9/13/2016 9:59 AM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Hello, Looks like program is in his first post. Best regards, Wizard |
9/13/2016 10:19 AM | |
Posts: 11 Rating:
|
sorry ... i att. the program in my first post .... |
This contribution was helpful to
1 thankful Users |
9/13/2016 2:54 PM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35964 Rating:
|
In the simulation I can not understand your mistakes. When the weekly timers B004 and B007 switches on, all 3 outputs are always switched with a time delay, first Q1, then Q2 and Q3 as the last. In the diagram is as hardware a 0BA6 selected and no 0BA2. I have cleaned up a bit the program. And made clearer. AttachmentSmall_House_Tmr_V2.zip (364 Downloads) |
This contribution was helpful to
1 thankful Users |
9/13/2016 3:31 PM | |
Posts: 11 Rating:
|
WOW !! very clear you'r V2 !! |
This contribution was helpful to
1 thankful Users |