4/7/2020 2:13 PM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi IOT2000 folks! Finally, the time has come! The successor of the IOT2040, the IOT2050, has been released and can be ordered via Siemens Mall. Some general information: There will be two versions of the IOT2050. The name IOT2050 is the same for both devices, just the MLFB is different. Both devices are based on an TI SOC AM65x8 64-bit ARM processor and will have a Display Port graphics interface. The main differences between the two versions are the following: 6ES7647-0BA00-0YA2 (IOT2050 Basic)
6ES7647-0BA00-1YA2 (IOT2050 Advanced)
These interfaces you know from the IOT2040 will remain:
OS options:
The difference is that the Simatic Industrial OS is system tested, there will be updates from Siemens incl. Security patches, there is easy installation of some packages with service stick, etc. More information about the Simatic Industrial OS can be found here It is already preinstalled incl. License on the 6ES7647-0BA00-1YA2. Already available documentation
To get started with the 6ES7647-0BA00-0YA2 you have to flash the Example Image to a µSD card, insert it and connect via SSH to 192.168.200.1 with interface X1P2. Best regards! |
Last edited by: bergmanu at: 04/07/2020 15:21:56Last edited by: bergmanu at: 04/15/2020 13:52:39Last edited by: bergmanu at: 04/29/2020 09:26:07Last edited by: bergmanu at: 04/29/2020 09:27:05Last edited by: bergmanu at: 07/26/2021 16:40:28Last edited by: bergmanu at: 09/30/2021 10:36:46Last edited by: bergmanu at: 09/30/2021 10:38:50Last edited by: bergmanu at: 11/24/2021 10:08:46Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to
14 thankful Users |
4/17/2020 4:33 PM | |
Posts: 80 Rating:
|
Hi bergmanu, When is going to be available the example image based on Debian? |
4/22/2020 9:03 AM | |
Joined: 3/1/2016 Last visit: 11/28/2023 Posts: 1 Rating:
|
According to https://mall.industry.siemens.com/mall/en/WW/Catalog/Product/6ES7647-0BA00-1YA2 the bigger one has 32 GB. |
Last edited by: Robsen at: 04/22/2020 09:04:36Last edited by: Robsen at: 04/22/2020 10:42:16 |
|
4/28/2020 3:39 AM | |
Joined: 9/8/2017 Last visit: 6/12/2020 Posts: 2 Rating:
|
This is needed as soon as possible: A documentation about Setting Up the IOT2050 will follow soon. |
4/29/2020 9:31 AM | |
Joined: 6/17/2014 Last visit: 10/27/2021 Posts: 77 Rating:
|
Hi, Can you tell me when version 2.0 of SIMATIC INDUSTRIAL OS will be available? Thanks in advance |
5/9/2020 10:36 AM | |
Joined: 4/28/2015 Last visit: 3/12/2025 Posts: 578 Rating:
|
If you have a rainy weekend and would like to build your own image: https://github.com/siemens/meta-iot2050 Binary release will follow. |
This contribution was helpful to
2 thankful Users |
5/18/2020 12:08 PM | |
Posts: 8 Rating:
|
Excellent, look forward to this. Been working with the 2040 and while its OK, a Debian based OS will be so much easier. Fingers crossed! |
6/11/2020 12:30 AM | |
Posts: 22 Rating:
|
[snip] Where is the example Image to get started with the Basic IoT2050 device? [snip] Thank you for help in advance [please use mutiple topics for different questions. You can find your other questions here: Question Regarding Reset button How to program H1300 (USER1) and H3300 (USER2) LEDs? IOT2050; function of the SIM Card slot? IO Shield accessories: Are they available to order just yet? plans to release PN Driver for IOT2050? |
Last edited by: NISARG at: 06/11/2020 00:32:42Last edited by: The Helping Hand at: 06/12/2020 10:34:00Split post into several (multiple questions) |
|
6/16/2020 8:20 AM | |
Joined: 8/31/2009 Last visit: 3/12/2025 Posts: 3 Rating:
|
Why is no image preinstalled ?!? 6ES7647-0BA00-1YA2 should be pre-installed ? |
7/10/2020 7:52 AM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, this was released one month ago. https://support.industry.siemens.com/tf/ww/en/posts/238945/ Best regards! |
Last edited by: bergmanu at: 07/10/2020 07:53:34Not working for IOT2050 support anymore from March 1st, 2024. |
|