Default Header
(header konnte nicht geladen werden)
4/15/2022 8:15 AM | |
Joined: 4/15/2022 Last visit: 4/15/2022 Posts: 1 Rating:
|
Can anyone explain course / Fine control with example . I tried as per attached Siemens application example . I Assumed that the controller output is 50 % , the fine control valve operating is from 0-30 % and course control valve operating range is from 30-100 % . As per the formula , I did notget expected out . Pl help it
AttachmentAD353-118r2.pdf (1166 Downloads) |
Follow us on