(0)| 7/31/2025 4:16 PM | |
|
Joined: 7/26/2022 Last visit: 1/8/2026 Posts: 6 Rating:
|
Dear Community, I'm developing a custom made block to read diagnostic info from Danfoss FC302 drive. To read diagnostic interrupt I'm using RALRM (SFB54). AS input/output of RALRM I've the following data: - Mode : 1 To read all output Data - Status : 16#0 - LEN : 0 (The length of the extracted AINFO) I receive the data of TINFO (Destination area for OB start and management information) without problem, only AINFO is always empty with zeros as values. [Attached is] an extract of the block where I'm declaring AINFO and TINFO as static. Attachment0801_Block.txt (129 Downloads) |
Last edited by: Moderator_Lan at: 08/01/2025 07:13:13Code attached |
|
Follow us on