7/31/2020 5:07 PM | |
Joined: 9/21/2006 Last visit: 5/25/2023 Posts: 247 Rating:
|
I am trying to write an Edge app that will work with both WinCC Unified PC RT and a WinCC Unified Comfort Panel. Since the only open interface that the UCP supports right now is OpenPipe, that i s what I am trying to use. I can get my Edge app running on the UCP by following the volume mapping syntax described in https://support.industry.siemens.com/cs/us/en/view/109778780. However, I have less success in connecting to OpenPipe on the PC. My node.js application runs find when node.js is running directly in Windows. However, when running in the docker container, I either get errors when I specify the volume mapping in the docker run command, or I get ECONNREFUSED errors when I try to connect to the OpenPipe in my application. The docker run errors occur when I use:
The error is:
I have tried various variants of the syntax - in quotes, using / instead of \, with and without the HmiRuntime, but no joy. https://stackoverflow.com/questions/47801477/can-i-use-named-pipes-inside-containers suggests that connecting to a Windows named pipe may only be possible on late versions of Windows Server (I am using Windows 10 Pro Workstation). If anyone has figured out how to attach to a Windows named pipe from within a Linux docker container, I would appreciate your insight. |
8/5/2020 10:05 AM | |
Joined: 8/16/2017 Last visit: 8/19/2025 Posts: 4 Rating:
|
Hi mmckay, We are also investigating on this topic currently. I will give you an update a soon as we have any news. |
Follow us on