5/9/2019 12:08 PM | |
Joined: 9/22/2014 Last visit: 1/8/2024 Posts: 89 Rating: (13) |
Hi ToidentuVietNam, Please find below link and go through Topic " 4.2 Communication between H-CPU and plant PCs " https://support.industry.siemens.com/cs/ww/en/view/90885106 Hope this will help you to make communication between your H system and PC "If it is Helpfull than Please Rate it." Thanks Pratts23 Attachment66644434_H_Configurations_V12_en.pdf (354 Downloads) |
Last edited by: Jen_Moderator at: 05/09/2019 12:26:48Optimized link and added PDF as an attachment. |
|
This contribution was helpful to1 thankful Users |
5/18/2019 3:51 AM | |
Posts: 10 Rating: (0) |
|
3/17/2020 8:21 PM | |
Joined: 4/28/2015 Last visit: 10/10/2023 Posts: 3 Rating: (0) |
Did anyone have answer to this question? Please share here |
3/17/2020 9:31 PM | |
Joined: 9/27/2006 Last visit: 6/2/2024 Posts: 12259 Rating: (2670) |
Hello Mohammed; You can connect a S7-400H PLC (programmed in Simatic Manager, Step 7 v5.x) to a WinCC V1x, panel or runtime, (TIA Portal) by the use of a so-called Device Proxy: Combined configuration with WinCC (TIA Portal) and STEP 7 V5.x or Combined configuration with WinCC (TIA Portal) and STEP 7 (TIA Portel) in separate projects (Video) https://support.industry.siemens.com/cs/ww/en/view/73502293 In the following article you can find the procedure to make the connection to the WinCC TIA Portal follow the switchover of the CPUs in case of failure of the primary controller: Automatic HMI Connection Fail-over in TIA Portal with the S7-400H Hope this helps, Daniel Chartier |
7/9/2021 7:40 AM | |
Joined: 8/3/2017 Last visit: 5/3/2024 Posts: 1085 Rating: (53) |
Hi, did you try out the answer from dchartier?
Please try it out. If it won't work, please ask further. |
Please, check out the forum search to find already existing topics regarding your issue and to get some hints. |
|
Follow us on