2/3/2011 10:36 AM | |
Joined: 4/19/2008 Last visit: 5/28/2024 Posts: 1525 Rating: (159) |
Hi voluhar, Switch is not a Problem, Basically you need to define the PN/PN Coupler in to the Hardware Configuration of both side PLC. & according to that you have to conenct the Connection. here is the Manual for the PN/PN Coupler. look on the Chapter 3, 4 for configuration Detail |
Ammy |
|
8/25/2016 10:28 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by k.dev is split to a separate thread with the subject How to connect two CPU via Profinet and programming. Best regards |
Follow us on