9/7/2017 3:46 PM | |
Posts: 1 Rating: (0) |
I am trying to read and write parameters to the IFM IO-Link Master AL1010. I can read the cyclic data but i cant read or write the parameters from the IFM flow sensor SA4100. I have used the IO-Link_Call Function Block to read and write the Parameter for Medium (index 686). I have set all the parameter as follows ID =3, CAP=255, PORT = 1, Index = 686, sub-index=0, LEN = 8. If i set REQ to 1 and RD_WR to 1, nothing happens. can someone point me in the right direction. ------------------------------------------------------------------------------------------ |
Last edited by: fpasipamire at: 9/7/2017 3:48:23 PMLast edited by: The Helping Hand at: 9/8/2017 12:42:06 PMNew subject after splitting |
|
9/12/2017 4:52 PM | |
Joined: 7/7/2010 Last visit: 5/3/2024 Posts: 14680 Rating: (2350)
|
Page 39 of https://www.ifm.com/mounting/7391036UK.pdf says 255hex so you are absolutely right! Nice find.
|
science guy |
|
Follow us on