(1)| 6/12/2014 11:44 AM | |
|
Posts: 1368 Rating:
|
Hello, the first question is: do you need PROFINET communication? Otherwise, you also can use the "normal" TCP/IP communication and the T-blocks, For I-device, look here https://www.automation.siemens.com/mdm/default.aspx?DocVersionId=63972520715&Language=en-US&TopicId=62565472779 it is a good step-by-step comfiguration. As transfer area, you must configure 4 byte input "I"(->), and 4 byte output "Q" (<-). |
This contribution was helpful to
|
|
| 6/12/2014 1:10 PM | |
|
Posts: 59 Rating:
|
Its done Thanks it was quite helpful. regards pramod takkar
|
This contribution was helpful to
|
|
| 6/12/2014 1:11 PM | |
|
Posts: 1368 Rating:
|
perfect! |
| 12/24/2017 8:59 PM | |
|
Joined: 9/27/2006 Last visit: 12/5/2025 Posts: 12455 Rating:
|
Hello Patthan; I do not know how familiar with industrial networking terminology, but if you have a serial network that uses the terms "master" and "slave" such as Modbus or Profibus-DP, then it is easy to make the profinet designations clear: - a Profinet IO Controller acts much as a "master": it holds the network configuration, initiates communications and polls the slaves cyclically; it is also able to diagnose communication problems and exchange specific data acyclically. - a Profinet IO device works much as a "slave": it responds to poll queries by the master, and sends it diagnostic information in case of error. For (a lot) more information on the subject, please download this little manual from PI International, the Profinet System Description, and examine the screenshot below.<https://www.profibus.com/index.php?eID=dumpFile&t=f&f=51714&token=4ea5554cbb80a066e805a879116ead2a759c23c3 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 12/25/2017 5:50:49 PMLast edited by: dchartier at: 12/25/2017 5:52:02 PM |
|
This contribution was helpful to
|
|
Follow us on