9/23/2016 3:24 PM | |
Joined: 10/18/2014 Last visit: 11/28/2023 Posts: 95 Rating: (15) |
Hello all please find attached word file where you can find option how to create pack & go file of your HMI program backup. Use of Pack & go:- You can easily extract above pack & go file from your PC/ Desktop & download your application example in HMI easilywithout having TIA Portal Wincc softwarein your laptop. Pack & go will create one program application file which you can open & download to your HMI, only download is possible not editing in that program is possible & you can download to same HMI with same network parameter which you have programmed for that Pack & go application source. Try it, it is very useful application in Siemens HMI. AttachmentTIA Pack & Go for HMI.docx (7289 Downloads) |
Ganesh-0220 |
|
This contribution was helpful to7 thankful Users |
9/23/2016 3:49 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hi, and here the Restrictions! To transfer the “Pack&Go” file to the operator panel, the following conditions must be fulfilled: On the PC, from which the “Pack&Go” file shall be transferred, the following software must be installed: – SIMATIC ProSave can either be installed via the WinCC (TIA Portal) product DVD, or downloaded in \3\. – Microsoft Visual C++ 2010 Redistributable Package (x86) can be downloaded in \4\. – Microsoft .Net Framework 4.5 can be downloaded in \5\. The PC, from which the “Pack&Go” file shall be transferred, must be connected to the operator panel via a network. Transfer via routing is not possible. From: Regards |
This contribution was helpful to6 thankful Users |
9/24/2017 5:09 PM | |
Posts: 116 Rating: (2) |
Hi Christoph, I did download HMI via internet and it also do firmware upgrade . during install runtime, it got abort. with Pack & Go, will it help ? |
10/4/2017 6:52 AM | |
Joined: 5/16/2017 Last visit: 2/22/2024 Posts: 3 Rating: (0) |
i have creat pack and go file. but how it's download in hmi ,please share document about that |
10/4/2017 7:12 AM | |
Posts: 310 Rating: (18) |
Hello, Maybe below link help with you . With Regards, |
9/12/2018 12:08 PM | |
Posts: 2 Rating: (0) |
How to download PACK n GO file in HMI ???? |
Follow us on